Spectroscopy is the measurement of a quantity as a function of either wavelength or frequency. The interaction between a wavelength of light and a sample produces information that describes the chemical composition of that sample.
Different wavelengths travel different distances and penetrate different depths. As a result, spectroscopy can be applied to any variety of sub-surface measurements across a multitude of fields. Some examples of industries and types of analysis are listed below:
Medical:
blood and tissue analysis
Natural Resources:
oil and mineral exploration
Food:
ingredient authentication
Pharmaceutical:
raw chemical purity detection
Environmental:
air/water quality
Agricultural:
detecting ripeness levels
Any spectroscopic system requires the ability to select the wavelength of light. The Digital Micromirror Device (DMD) at the heart of DLP® technology allows the dynamic selection of various wavelengths of light through millions of independently controlled bi-state mirrors. This means that spectroscopic measurement systems no longer need to be designed with a fixed wavelength input. Instead, the DMD chip can help achieve a ‘tunable’ spectrometer that allows measurement of different materials using different wavelengths of light using the same spectrometer system. As a result, DLP® technology is gaining attention in various spectroscopy segments including molecular and atomic spectroscopy.