Hydraulic ValveHydraulic Valve |
|
Hydraulic ValveHydraulic Valve |
|
Block DiagramClick on the colored blocks to view or sample recommended solutions
Design ConsiderationsHydraulic Valve A hydraulic valve directs the flow of a liquid medium, usually oil, from its input ports to its output ports. The direction of the oil flow is determined by the position of a spool, which is driven by a linear force motor: The core subsystems include:
The valve controller receives a position-command from the fieldbus via the system controller and drives the linear force motor until the output signal of the position sensor (LVDT=Linear Variable Differential Transformer) equals the input value of the position command. At the same time, pressure and temperature are monitored. An alarm condition is indicated, if one of these sensors exceeds a pre-determined safety-value. Application NotesMost useful technical documents for Hydraulic Valve
|
|