|
|
Product InformationDescriptionSimpliciTI is a simple low-power RF network protocol aimed at small RF networks. Such networks typically contain battery operated devices which require long battery life, low data rate and low duty cycle and have a limited number of nodes talking directly to each other or through an access point or range extenders. Access point and range extenders are not required but provide extra functionality such as store and forward messages. With SimpliciTI the MCU resource requirements are minimal which results in the low system cost. SimpliciTI was designed for easy implementation and deployment out-of-the-box on several TI RF platforms such as the MSP430 family of low-power MCUs and the CC1XXX/CC25XX transceivers and SoCs. The sample applications run out-of-the-box on several hardware platforms:
Download & Register (To Receive Update Notifications via e-mail)SimpliciTI-1.1.0.exe for CC11xx, CC25xx and CC2x30 using IAR EW430 or EW8051 SimpliciTI-CCE-1.1.0.exe for CC1101, CC2500, CC2520 and CC430 using CCE for MSP430 Hot new features in version 1.1.0 includes:
By registering, we will be able to notify you of updates when they become available and provide instructions on how to perform the update. Check out the TI Packet Sniffer for SimpliciTI below The packet sniffer runs on CC2510DK/CC1110DK and can visualize the traffic on air in real-time. The Sensor Network Analyzer from Daintree has been enhanced to provide decode and analysis support for SimpliciTI. Features
Compatibility IssuesTools: SimpliciTI is supplied as full source code and the supplied projects can be compiled using the CCE and IAR EW430 for MSP430 or EW8051 for 8051 SoCs. Evaluation versions of the IAR compilers can be downloaded from www.iar.com. Small applications can be built using the free evaluation version. Please contact your local IAR office for further details. 30-day evaluation license for the Sensor Network Analyzer from Daintree available to new users. In order to use the Daintree Sensor Network Analyzer (SNA) software, a packet sniffer compliant hardware module is needed. The SNA software works with hardware included in the CC2520DK, CC2430(Z)DK, CC2431(Z)DK, and CC2530(Z)DK. Technical DocumentsMost useful technical documents for SIMPLICITI More Literature
|
| Related Tools | |||
| Name | Part# | Company | Tool Type |
| CC1101 Development Kit 433MHz | CC1101DK433 | Texas Instruments | Development Boards/EVMs |
| CC1101 Development Kit 868-915MHz | CC1101DK868-915 | Texas Instruments | Development Boards/EVMs |
| CC1110 and CC1111 Development Kit | CC1110-CC1111DK | Texas Instruments | Development Boards/EVMs |
| CC2430 Development Kit | CC2430DK | Texas Instruments | Development Boards/EVMs |
| CC2500/CC2550DK Development Kit | CC2500-CC2550DK | Texas Instruments | Development Boards/EVMs |
| CC2510/CC2511 Development Kit | CC2510-CC2511DK | Texas Instruments | Development Boards/EVMs |
| CC2520 Development Kit | CC2520DK | Texas Instruments | Development Boards/EVMs |
| CC2530 Evaluation Module Kit | CC2530EMK | Texas Instruments | Development Boards/EVMs |
| CC2591EMK Evaluation Module Kit | CC2591EMK | Texas Instruments | Development Boards/EVMs |
| MSP430FG4618/F2013 Experimenter Board | MSP-EXP430FG4618 | Texas Instruments | Development Boards/EVMs |
| CC2530 Development Kit | CC2530DK | Texas Instruments | Development Platforms |
| Sensor Network Analyzer from Daintree | SENSOR_NETWORK_ANALYZER_FROM_DAINTREE | Daintree Networks, Inc. | Software Tools |
| Related Devices | |||
| Part# | Name | Product Family | |
| CC1100 | Highly Integrated MultiCh RF Transceiver Designed for Low-Power Wireless Apps | Low Power RF ICs | |
| CC1100E | Low-Power Sub-1GHz RF Transceiver for China and Japan frequency bands | Low Power RF ICs | |
| CC1101 | Low-Power Sub-1GHz RF Transceiver | Low Power RF ICs | |
| CC1110F16 | Sub-1GHz System-on-Chip with MCU and 16kB Flash memory | Low Power RF ICs | |
| CC1110F32 | Sub-1GHz System-on-Chip with MCU and 32kB Flash memory | Low Power RF ICs | |
| CC1110F8 | Sub-1GHz System-on-Chip with MCU and 8kB Flash memory | Low Power RF ICs | |
| CC1111F16 | Sub-1GHz System-on-Chip with MCU, 16kB Flash memory and USB 2.0 | Low Power RF ICs | |
| CC1111F32 | Sub-1GHz System-on-Chip with MCU, 32kB Flash memory and USB 2.0 | Low Power RF ICs | |
| CC1111F8 | Sub-1GHz System-on-Chip with MCU, 8kB Flash memory and USB 2.0 | Low Power RF ICs | |
| CC2430 | System-on-Chip Solution for 2.4 GHz IEEE 802.15.4 / ZigBee™ | Low Power RF ICs | |
| CC2500 | Low Cost, Low-Power 2.4 GHz RF Transceiver Designed for Low-Power Wireless Apps in the 2.4 GHz ISM B | Low Power RF ICs | |
| CC2510F16 | 2.4 GHz Radio Transceiver, 8051 MCU and 16 kB Flash memory | Low Power RF ICs | |
| CC2510F32 | 2.4 GHz Radio Transceiver, 8051 MCU and 32 kB Flash memory | Low Power RF ICs | |
| CC2510F8 | 2.4 GHz Radio Transceiver, 8051 MCU and 8 kB Flash memory | Low Power RF ICs | |
| CC2511F16 | 2.4 GHz Radio Transceiver, 8051 MCU, 16 kB Flash memory and full-speed USB interface | Low Power RF ICs | |
| CC2511F32 | 2.4 GHz Radio Transceiver, 8051 MCU, 32 kB Flash memory and full-speed USB interface | Low Power RF ICs | |
| CC2511F8 | 2.4 GHz Radio Transceiver, 8051 MCU, 8 kB Flash memory and full-speed USB interface | Low Power RF Protocols | |
| CC2520 | Second generation 2.4 GHz ZigBee/IEEE 802.15.4 RF transceiver | Low Power RF Protocols | |
| CC2530 | Second Generation System-on-Chip Solution for 2.4 GHz IEEE 802.15.4 / RF4CE / ZigBee | Low Power RF ICs | |
| CC2591 | 2.4 GHz RF Front End | Low Power RF ICs | |
Most Popular Tags for SIMPLICITI: