C28x Fast Fourier Transforms Library Status: ACTIVE

SPRC081


      
         
  SPRC081
NameC28x Fast Fourier Transforms Library
StatusACTIVE
Price (US$)Free 
Host  PC 
OS  Win NT/98/2000/ME/XP 
Current Version  v0.9b 
Version Date  08/17/2004 
Order Options


Product Information

Description

Fast Fourier Transforms are an efficient class of algorithms for the digital computation of the N-point Fourier transform (DFT). In general, their input sequence are assumed to be complex. In many real applications, the data sequences to be processed are real valued. Even though the data is real, complex-valued DFT algorithm can still be used. One simple approach creates a complex sequence from the real sequence; that is, real data for the real components and zeros for the imaginary components, The complex FFT can then be applied directly.

However, this method is not efficient as it consumes 2N memory locations (Real & Imaginary) for N point sequence. When input is purely real, their symmetric properties compute DFT very efficiently. One such optimized real FFT algorithm for 2N-point real data sequence is packing algorithm. The original 2N-point sequence is packed as N-point complex sequence and N -point complex FFT is performed on the complex sequence. Finally the resulting N -point complex output is unpacked into another N+1 point complex sequence, which corresponds to spectral bin 0 to N of 2N-point real input sequence. Spectral bin 0 to N is sufficient, as the remaining bins N+1 to 2N-1 are complex conjugates of spectral bins N-1 to 1.

The real FFT requires 2N+2 memory locations to compute the FFT for 2N-point real valued sequence, which is highly preferable in contrast to the complex FFT that consumes 4N-locations for 2N-point real valued sequence. Moreover using this strategy, the complex FFT size can be reduced by half, at the FFT cost function of O(N) operations to pack the input and unpack the output. Hence, the real FFT algorithm computes the FFT of a real input sequence almost twice as fast as the general FFT algorithm.

This FFT library contains generic FFT module (32-bit implementation) for real/complex FFT.


Note:

  • Documentation of FFT Modules is archived in the self-extracting zip file, and the pdf files can be found in c:\tidcs\c28\dsp_tbox\fft\doc directory.

  • Software Test Bench (STB) support library must be downloaded to use the STB examples.


Order Options

 SPRC081
Name C28x Fast Fourier Transforms Library
Status  ACTIVE 
Price (US$) Free 
 

    
Related Devices
Part# Name Product Family
TMS320C2801 32-Bit Digital Signal Controller with ROM C2000™ 32-bit Real-time MCUs 
TMS320C2802 32-Bit Digital Signal Controller with ROM C2000™ 32-bit Real-time MCUs 
TMS320F2802 32-Bit Digital Signal Controller with Flash C2000™ 32-bit Real-time MCUs 
TMS320F2809 32-Bit Digital Signal Controller with Flash C2000™ 32-bit Real-time MCUs 

Support and Community

Customer Tags Help

Most Popular Tags for SPRC081:

View All Tags