Multimedia Framework Products (MFP) - Codec Engine and xDAIS Framework Components Status: ACTIVE

TMDMFP

      
         
  TMDMFP
NameMultimedia Framework Products (MFP) - Codec Engine and xDAIS Framework Components
StatusACTIVE
Price (US$) 

Product Information

Description

Multimedia Framework Products (MFP)

A major advantage of programmable DSPs over fixed-function devices is their ability to accelerate multiple multimedia functions in a single device. TI multimedia framework products are designed to enable users to easily share a DSP between algorithms by handling issues like data buffer cache coherency, DMA resource contention, and efficient use of scratch memory. Developers can then leverage their application-specific expertise to create differentiated products.

TI provides both a codec execution framework, known as Codec Engine, as well as lower-level components for developers who wish to create an eXpressDSP-compliant framework from scratch. If you previously used TI References Frameworks (such as RF5), please contact TI for information on these.

Features

Multimedia Framework Products (MFP) - Codec Engine and xDAIS Framework Components

Codec Engine - Codec Engine is a codec execution framework that automates the invocation and instantiation of eXpressDSP-compliant codecs and algorithms. Codec Engine can execute in ARM-only, ARM-DSP, or DSP-only environments and supports concurrent execution of multiple channels and codecs. It does not provide A/V synchronization or manage application I/O, but rather accepts and delivers elementary audio and video streams. Codec Engine is designed to be used in conjunction with higher layer frameworks or middleware that provide a/v synchronization, video port and disk I/O, or network streaming while calling Codec Engine's eXpressDSP-compliant APIs for actual encoding, decoding, and processing. This approach enables system providers to easily differentiate their applications while still leveraging Codec Engine.

In the ARM environment, Codec Engine is currently ported to the Linux operating system. Contact your TI sales representative to inquire about availability of Codec Engine for other ARM operating systems. In DSP environments, Codec Engine uses the DSP/BIOS operating system. Codec Engine performs the following functions:
  • Automated dynamic instantiation of eXpressDSP-compliant codecs, including creation of a DSP/BIOS task to execute the codec and providing DMA and scratch memory resources as requested by the codec through the IALG and IDMA interfaces. Codec Engine simplifies the task of efficiently executing multiple codecs on a single DSP.
  • Transparent execution of codecs regardless of where the application resides with the respect to the codecs. In some ARM-DSP applications, it may be desirable to execute audio codecs, for example, on the ARM and video codecs on the DSP. In addition, developers may have multiple versions of an application code base, some using ARM-DSP based devices and others using DSP-only devices. Codec Engine provides the same application interface for invoking a codec regardless of whether the codec resides on the same core or whether it needs to be invoked remotely on a DSP from an ARM. Codec Engine automatically handles the remote invocation and execution and any required cache management for the data buffers.
  • Codec Engine provides APIs for acquiring system resource data, such as DSP CPU and memory usage by codecs. Developers can view this system resource data using the Eclipse-based Data Visualization Toolkit.
  • Codec Engine provides standardized configuration tooling for creating the codec combinations needed for a specific application.
xDAIS Framework Components - For developers who prefer complete control over application development, TI also provides low-level components that enable a framework to easily interact with eXpressDSP-compliant algorithms. xDAIS Framework Components query algorithms for their memory and DMA resource requirements and then enable sharing of resources if desirable. xDAIS Framework Components include the following three modules:
  • DSKT: DSKT uses the xDAIS IALG interface to determine what system memory resources they require and then allocates the memory while instantiating the codec.
  • DMAN3: DMAN uses the xDAIS IDMA3 interface to determine which DMA resources are required by a codec. DMAN3 includes several enhancements to take full advantage of the DMA (including QDMA and EDMA 3.0) capabilities offered by the 64+ core.
  • ACPY3: ACPY3 is commonly used by video codecs that frequently perform memory-to-memory copies. ACPY3 performs fast DMA-based memory-to-memory copies using DMA resources acquired through DMAN3. ACPY3 is highly optimized to deliver maximum performance for 64+ devices.

Multimedia Framework Products (MFP) - Downloads

Multimedia Framework Products (MFP) - includes the following:

Technical Documents

Most useful technical documents for TMDMFP Help

Datasheet

Application Notes

User Guides

    
Related Software
Name Part# Company Software Type
AAC HE and LC Audio Decoder TMDAACD Texas Instruments Algorithms / Codecs 
AAC HE and LC Audio Encoder TMDAACE Texas Instruments Algorithms / Codecs 
H.264 Video Decoder TMDH264D Texas Instruments Algorithms / Codecs 
H.264 Video Encoder TMDH264E Texas Instruments Algorithms / Codecs 
JPEG Imaging Decoder TMDJPEGD Texas Instruments Algorithms / Codecs 
JPEG Imaging Encoder TMDJPEGE Texas Instruments Algorithms / Codecs 
MP3 Audio Decoder TMDMP3D Texas Instruments Algorithms / Codecs 
MP3 Audio Encoder TMDMP3E Texas Instruments Algorithms / Codecs 
MPEG-2 Video Decoder TMDMPEG2D Texas Instruments Algorithms / Codecs 
MPEG-2 Video Encoder TMDMPEG2E Texas Instruments Algorithms / Codecs 
MPEG-4 Video Decoder TMDMPEG4D Texas Instruments Algorithms / Codecs 
MPEG-4 Video Encoder TMDMPEG4E Texas Instruments Algorithms / Codecs 
eXpressDSP Algorithm Standard – xDAIS Developer’s Kit and xDM TMDXDAISXDM Texas Instruments Algorithms / Codecs 
Related Tools
Name Part# Company Tool Type
Digital Video Software Development Kit, based on DaVinci™ Technology TMDSSDK6446 Texas Instruments Development Platforms 
Related Devices
Part# Name Product Family
OMAP-L137 Low-Power Applications Processor OMAP™ Applications Processors 
TMS320C6743 Fixed/Floating-Point Digital Signal Processor C6000™ Floating-point DSPs 
TMS320C6745 Floating-Point Digital Signal Processor C6000™ Floating-point DSPs 
TMS320C6747 Floating-Point Digital Signal Processor C6000™ Floating-point DSPs 
TMS320DM335 Digital Media System-on-Chip (DMSoC) DaVinci™ Digital Media Processors 
TMS320DM355 Digital Media System-on-Chip (DMSoC) DaVinci™ Digital Media Processors 
TMS320DM357 Digital Media System-on-Chip (DMSoC) DaVinci™ Digital Media Processors 
TMS320DM6431 Digital Media Processor DaVinci™ Digital Media Processors 
TMS320DM6433 Digital Media Processor DaVinci™ Digital Media Processors 
TMS320DM6435 Digital Media Processor DaVinci™ Digital Media Processors 
TMS320DM6437 Digital Media Processor DaVinci™ Digital Media Processors 
TMS320DM6441 DaVinci Digital Media System-on-Chip DaVinci™ Digital Media Processors 
TMS320DM6443 DaVinci Digital Media System-on-Chip DaVinci™ Digital Media Processors 
TMS320DM6446 DaVinci Digital Media System-on-Chip DaVinci™ Digital Media Processors 
TMS320DM6467 Digital Media System-on-Chip DaVinci™ Digital Media Processors 
TMS320DM647 Digital Media Processor DaVinci™ Digital Media Processors 
TMS320DM648 Digital Media Processor DaVinci™ Digital Media Processors 

Support and Community

Customer Tags Help

Most Popular Tags for TMDMFP:

View All Tags

Other Support