TUSB2136-TPS2149 Product Development Kit Status: ACTIVE

TUSB2136TPS2149PDK


      
         
  TUSB2136TPS2149PDK-FW TUSB2136TPS2149PDK
NameTUSB2136 Firmware Source CodeTUSB2136-TPS2149 Product Development Kit
StatusACTIVEACTIVE
Price (US$)Free $149.00 
Order Options

Order Options


Product Information

Description


View  View TUSB2136TPS2149PDK Graphic

The TUSB2136TPS2149PDK can be used to evaluate the TUSB2136 USB compound hub device and the TPS2149 USB power controller device in a keyboard application. Both a main evaluation module and a mini keyboard are included in the TUSB2136TPS2149PDK. The user is expected to be familiar with 8052 MCU architecture and programming, as well as USB certification requirements. For more information on Universal Serial Bus and certification, logo, and testing requirements, see www.usb.org.

Software/Utilities Available include:

  • AppLoader is a Windows-based USB Device Driver that will load binary 8052 code to the TUSB2136. It allows the user to keep the firmware on the PC rather than in an EEPROM on the board. The EEPROM must be removed from the board for Apploader to function. When the device is plugged into the PC, Windows associates it with this driver, which then downloads the firmware to the device's RAM directly. AppLoader has been tested under Win98SE, Win2K, WinME and WinXP. It is intended to be used during the firmware development phase of a project and is not intended for production use. Firmware on production systems should be stored on an EEPROM in the USB device.
  • The I2C Header Generator Utility is a DOS-based tool that generates an image file for your I2C EEPROM, using your binary object code and/or custom descriptors as inputs.
  • The Sample Source Code can be downloaded if you agree to the online royalty-free license agreement. Objext code comes pre-loaded in the on-board EEPROM. If you will do your own firmware devlopment, a Compiler will be required. Since the TUSB2136 is based upon the industry-standard 8052 microcontroller, there are several compilers on the market that would be suitable. Some examples are at www.iar.com, www.keil.com, and at www.tasking.com.

The TUSB2136/3210 Firmware Debugging Guide is a general instruction guide on how to debug user-developed firmware using the TUSB2136's native 8052 debug port.

The TUSB2136/3210/5052 USB Firmware Architecture 8052 Embedded USB Micro-Controller document discusses the firmware architecture of the TUSB3210.

Additional items needed for EVM use include a USB Montioring Utility and a USB enabled Host computer.

Features

  • Facilitate Development with a resident TUSB2136 USB micro-controller
  • Test the on-board TPS2149 power controller
  • Quick keyboard testing via mini input keys
  • Connection to a USB-enabled host

What's Included

  • Data Manual
  • Downloadable App Loader
  • Downloadable I2C Header Generator Utility
  • Downloadable gerber file
  • Getting Started Letter
  • Mini-Keyboard Daughter Card
  • Populated EVM Board
  • Sample Source Code
  • Schematic
  • User's Guide

Support Software

Compatibility Issues

This kit assumes that the human interface device (HID) class drivers native to all major operating systems will be utilized. If the HID class driver (or other native class driver) is not satisfactory, the user will be required to develop their own driver.

Order Options

 TUSB2136TPS2149PDK-FWTUSB2136TPS2149PDK
Name TUSB2136 Firmware Source CodeTUSB2136-TPS2149 Product Development Kit
Status  ACTIVE ACTIVE 
Price (US$) Free $149.00 
 

Order
 Americas:
Contact Distributor

Asia:
Contact Distributor

Europe:
Contact Distributor

Japan:
Contact Distributor
 

Technical Documents TI Recommends - Technical Documentation TI Recommends

Most useful technical documents for TUSB2136TPS2149PDK Help

Datasheet

Application Notes

User Guides

More Literature

    
Related Devices
Part# Name Product Family
TPS2149 3.3V LDO + Dual Switch For USB Hubs, Active-Low Enables PCMCIA and USB 
TUSB2136 Universal Serial Bus Compound Hub With General-Purpose 8052 MCU USB 
TUSB3210 Universal Serial Bus General-Purpose Device Controller USB 

Support and Community

Customer Tags Help

No Tags are Available for this Part Number

Other Support