TUSB3210 Keyboard Product Development Kit Status: ACTIVE

TUSB3210KBDPDK


      
         
Getting Started Documentation   TUSB3210 Keyboard Evaluation Board (Rev. A) (HTM 8 KB) 1438 views
17 Jun 2003 Read Abstract

  TUSB3210KBDPDK-FW TUSB3210KBDPDK
NameTUSB3210 Firmware Source CodeTUSB3210 Keyboard Product Development Kit
StatusACTIVEACTIVE
Price (US$)Free $199.00 
Order Options

Order Options


Product Information

Description


View  View TUSB3210KBDPDK Graphic

The TUSB3210KBDPDK can be used to evaluate the TUSB3210 in a keyboard application. For evaluation of the TUSB3210 as a general purpose USB micro-controller (MCU), please see the TUSB3210GENPDK. The user is expected to be familiar with 8052 MCU architecture and programming, as well as USB certification requirements. For more information on Universal Serial Bus and certification, logo, and testing requirements, see www.usb.org.

Software/Utilities Available include:

  • The I2C Header Generator Utility is a DOS-based tool that generates an image file for your I2C EEPROM, using your binary object code and/or custom descriptors as inputs. It is not capable of programming the EEPROM, only formatting the file correctly for use with an external 3rd party programmer.
  • The Sample Source Code can be downloaded if you agree to the online royalty-free license agreement. Object code comes pre-loaded in the on-board EEPROM. If you want to do your own firmware development, a Compiler will be required. Since the TUSB3210 is based upon the industry-standard 8052 microcontroller, there are several compilers on the market that would be suitable. Some examples are at www.iar.com, www.keil.com, and at www.tasking.com.

The TUSB2136/3210 Firmware Debugging Guide is a general instruction guide on how to debug user-developed firmware using the TUSB3210's native 8052 debug port.

The TUSB2136/3210/5052 USB Firmware Architecture 8052 Embedded USB Micro-Controller document discusses the firmware architecture of the TUSB3210.

Additional items needed for EVM use include a USB Montioring Utility and a USB enabled Host computer.

Features

  • Facilitate development with a resident TUSB3210 USB micro-controller
  • Ready keyboard test via mini input keys
  • Connection to a USB-enabled host

What's Included

  • Downloadable I2C Header Generator Utility
  • Downloadable gerber file
  • Getting Started Letter
  • Populated EVM Board
  • Schematic
  • USB Cable
  • User's Guide

Support Software

Compatibility Issues

This kit assumes that the human interface device (HID) class drivers native to all major operating systems will be utilized. If the HID class driver (or other native class driver) is not satisfactory, the user will be required to develop their own driver.

Order Options

 TUSB3210KBDPDK-FWTUSB3210KBDPDK
Name TUSB3210 Firmware Source CodeTUSB3210 Keyboard Product Development Kit
Status  ACTIVE ACTIVE 
Price (US$) Free $199.00 
 

Order
 Americas:
Contact Distributor

Asia:
Contact Distributor

Europe:
Contact Distributor
 

Technical Documents TI Recommends - Technical Documentation TI Recommends

Most useful technical documents for TUSB3210KBDPDK Help

Datasheet

Application Notes

User Guides

    
Related Tools
Name Part# Company Tool Type
TUSB3210GENPDK Generic Product Development Kit TUSB3210GENPDK Texas Instruments Development Boards/EVMs 
Related Devices
Part# Name Product Family
TUSB2136 Universal Serial Bus Compound Hub With General-Purpose 8052 MCU USB 
TUSB3210 Universal Serial Bus General-Purpose Device Controller USB 

Support and Community

Customer Tags Help

No Tags are Available for this Part Number

Other Support