DaVinci/OMAP System Integration Workshop using Linux
 Training Home TRAINING HOME
DETAILS
LOGISTICS

Duration
4 Days


  OVERVIEW   

The DaVinci/OMAP System Integration using Linux workshop covers the development of a generic video application.  This application is being used because the peripherals on these first DaVinci devices were chosen to greatly accelerate the video applications (and their development).  However these concepts can easily be applied to other types of systems. Other processors discussed are the DM646x, DM3xx, OMAP35x and OMAP-L1xx processors Beginning with an overview of the device architecture, this workshop will use a generic video system to explore the various DM644x hardware peripherals and software components. The workshop will concentrate on the various software components provided by Texas Instruments: device drivers, Codec Engine (interprocessor communication framework), xDM (codec/algorithm interface standard). At the end of the workshop, attendees will have the opportunity to use and evaluate a variety of advanced system design/debug details.

 

Workshop Outline

 

1. Introduction to DaVinciTM Technology: Device, Software, and Tools

  • Video system overview
  • Device system architecture
  • Introduction to the software architecture (Codec Engine, xDM)
  • Overview of tools

2. Application Layer Programming

  • Getting data in/out of the system
    • Intro to device drivers
    • Using a hard disk drive
    • Using the audio serial port
    • Using the video capture/display drivers (V4L2,FBdev)
  • Adding ARM®-based (local) processing to the Input/Output thread
  • Moving real-time processing tasks to the DSP (remote processing)

3. Signal Processing Layer Programming

  • Using the xDM interfaces to write signal processing algorithms
    • ARM/Linux-based processing
    • DSP-based processing
  • Packaging signal processing content for easy configuration and re-use

4. Advanced System Programming Details

  • Advanced System Configuration - Using the DVSDK
    • Using the config tool to easily substitute codec algorithms
    • Changing the priorities of processing tasks running on the DSP
  • Using the CE trace features
  • Using the SoC Analyzer to evaluate system performance

 

About DaVinci Technology-Based TMS320DM644x Digital Media Processors

DaVinci technology is optimized for digital video systems and includes DSP-based SoCs, multimedia codecs, APIs, frameworks and development tools. These integrated components are the industry's first complete offering of an open platform for video system development.

This workshop focuses on the DM644x architecture, which is a highly integrated SoC that has absorbed many of the external components required for digital video. The DM644x processors, available today, are based on the TMS320C64x+TM DSP core and ARM926 processor and include video accelerators, networking peripherals and external memory/storage interfaces all specifically tuned for video.

TMS320DM6443 digital media processor is tuned for video decode applications and provides all of the processing components required to decode digital video.

TMS320DM6446 digital media processor, tuned for encode and decode applications, adds video encoding capabilities through a dedicated video processing front-end capable of capturing various digital video formats.

Not sure which workshop is best for you? Use the Selection Tools listed below

Workshop Selection Tool

Processor-to-Workshop Selection Tool

 

Who Should Attend

The course has been designed for software and system engineers who are planning to use the Texas Instruments DM644x, DM646x, DM3xx, OMAP35x and OMAP-Llxx devices.

The workshop addresses building a system using the various software drivers and framework components provided by Texas Instruments including: 

  • ARM running MontaVista Linux
  • DSP running DSP/BIOSTM kernel
  • Signal processing and interprocessor communication (IPC) via Codec Engine (VISA API)
  • Signal Processing Layer (codecs and algorithms) built using xDM/xDAIS API 
  • Real-Time software components (codecs, Servers, Engines) packaged with XDC tool

Prerequisites

While these prerequisites are note officially required, we offer them as guidance for the skills used in this workshop.  Enhancing your knowledge in these areas before the workshop should help you get the most from your Texas Instruments' workshop experience. 

Required

  • Working knowledge of C programming - This is the primary computer language used for  this course. If you are not actively programming in C on a regular basis, we suggest that you refresh your C programming knowledge through a book or course prior to attending the workshop.

Not required, but highly recommended

  • Basic Linux OS skills (i.e. shell commands, etc.)
  • Embedded system basics (what is a memory map, linking, etc.) 

Nice to have   

  • TMS320C64xTM DSP Programming
  • Basic Linux programming (processes, threads, etc.)
  • Understanding of Linux device drivers
  • Video Application/System knowledge

What is not covered in the workshop

Please note that this course was not designed for hardware layout/design engineers. While the material may prove useful to hardware engineers, the course does not address their specific needs. These concerns are being addressed through a series of application notes and reference designs. Please contact your local TI representative (or the Product Information Center - support@ti.com) if you have further questions.

  

How can attending a Texas Instruments Workshop help you with your project?

See what our customers are saying....

"This workshop greatly reduces the learning curve and provides a good view of where to start and what is available."

 

"This workshop is wonderfully organized. The lab progression is excellent. It was a great experience."

 

"This workshop has helped me get a complete grasp of the DaVinci. I have a board and have been coding it some before this point. The course helped solidify my understanding."  

 

"This workshop has taught me, in a very short time, all the things that the DaVinci technology can do for me. Now I have confirmation that our choice of DaVinci is an excellent match for our project needs."   

 

Workshop Comparison Chart 

 

Workshop Applicable Devices Primary OS Peripheral programming Framework or Example Code Algorithms Interrupts Cache DMA Flash Stand-alone system
DaVinci/OMAP System Integration using Linux 

DM644x, DM646x, DM3xx, OMAP35x

OMAP-L1xx

Linux PSP Linux drivers Codec Engine call xDM codecs/algorithms N/A N/A ACPY3  
TMS320C64x+™ DSP System Integration using DSP/BIOS

DM643x, C642x,

C674x

DM647, DM648

DSP/BIOS PSP BIOS drivers Framework Components (DSKT, DMAN, ACOPY) call xDAIS or xDM algorithms Yes Yes DSKT and DMAN framework components Yes

TMS320C645x DSP System Integration Workshop 

 

C645x DSP/BIOS CSL 3.0, NDK, SRIO   none Yes Yes EDMA 3.0 details yes
TMS320C6000 DSP Optimization Workshop  All C6000, detailed CPU architecture Not Applicable Not Applicable  Not Applicable create a XDAIS algorithm Yes  Yes brief discussion  Not Applicable
TMS320C28x™ DSP Workshop  F283xx, F282xx, F281x, F280x No OS or DSP/BIOS C header files Programming examples none Yes   C28x DMA examples yes

Back to Top

Processor-to-Workshop Selection Chart

 

Processor Platforms Processors Recommended Workshop Tool used
DaVinci™ Digital Media Processors TMS320DM644x DaVinci/OMAP System Integration using Linux  DM6446 EVM
  TMS320DM646x DaVinci/OMAP System Integration using Linux  DM6446 EVM
  TMS320DM3xx DaVinci/OMAP System Integration using Linux  DM6446 EVM
  TMS320DM643x TMS320C64x+™ DSP System Integration using DSP/BIOS DM6437 EVM
  TMS320DM647 TMS320C64x+™ DSP System Integration using DSP/BIOS DM6437 EVM
  TMS320DM648  TMS320C64x+™ DSP System Integration using DSP/BIOS DM6437 EVM
OMAP™ Applications Processors OMAP35x™ DaVinci/OMAP System Integration using Linux  DM6446 EVM
  OMAP-L1xx DaVinci/OMAP System Integration using Linux  DM6446 EVM
TMS320C6000TM  DSPs TMS320C645x™ TMS320C645x DSP System Integration Workshop  6455 EVM
  TMS320C642x™ TMS320C64x+™ DSP System Integration using DSP/BIOS DM6437 EVM
  TMS320C67x™ TMS320C64x+™ DSP System Integration using DSP/BIOS DM6437 EVM
  TMS320C672x™ TMS320C64x+™ DSP System Integration using DSP/BIOS DM6437 EVM
TMS320C2000™ Digital Signal Controllers TMS320F283xx TMS320C28x™ DSP Workshop  F28335 eZdsp
  TMS320F282xx  TMS320C28x™ DSP Workshop  F28335 eZdsp
  TMS320F281x  TMS320C28x™ DSP Workshop  F28335 eZdsp
  TMS320F280x TMS320C28x™ DSP Workshop  F28335 eZdsp

 

Back to top

Workshop Pricing 

United States    $1595.00                        Register Now    

Dec 08-11, 2009     Dallas, TX

Feb 02-05, 2010     San Diego, CA

Feb 23-26, 2010     Dallas, TX

Mar 23-26, 2010     Chicago, IL

Apr 13-16, 2010     Waltham, MA

May 18-21, 2010    Sunnyvale, CA

Jun 22-25, 2010      Dallas, TX

 

 

 

Europe            €1800 excluding VAT       Register Now 

No classes currently available

 

Israel              $950                                 Register Now 

No classes currently available

 

China            RMB 3000 tax included    Register Now 

Licensed to be taught by SEED   合众达电子  

No classes currently available

 

 

   

Taiwan         NT$ 26775 tax included      Register Now 

No classes currently available

 

Rest of Asia   US$ 750 tax excluded      Register Now 

 (excluding Korea and Japan)

No classes currently available

 

Workshops are conducted in the following languages:

  • All European and USA Multi-day workshops are conducted in English
  • Workshops in Korea are conducted in Korean
  • Workshops in Japan are conducted in Japanese
  • Workshops in China and Taiwan are conducted in Mandarin Chinese
  • Workshops in other parts of Asia are conducted in English

 

Course Details

Classes begin at 8:30 a.m. and run through 5:30 p.m. each day. You can expect to finish class between  2:00pm and 4:00pm on the final day. 

Cancellation Policy

  • European classes are subject to cancellation if minimum number of attendees is not  met one week prior to the date of the workshop.  
  • US classes are subject to cancellation if minimum number of attendees is not met two weeks prior to  the date of the workshop.

   Minimum = 5   Maximum = 12