Subscribe to the Automotive Solutions eNewsletter.

March 2006
In this issue:
 
Semiconductors
Car Audio Amplifiers From TI Deliver
90 Percent Power Efficiency
TI Enables New Automotive Jukebox Market With High-Speed Ripping Capabilities
New Automotive LVDS Serializer/Deserializer Less Than One-Third the Size of Competing Devices
OMAP™ Technology and TI Third Parties Drive Automotive Applications

Automotive Articles
Data and Audio Processing for HD Radio

Semiconductors

Car Audio Amplifiers From TI Deliver 90 Percent Power Efficiency

TI Car Audio SolutionsUshering in a higher standard in car audio, TI announced its first digital amplifiers designed to meet the high reliability and unique requirements of the automotive market. The TAS5414 and TAS5424 Class D amplifiers introduce the power efficiency of digital amplification for automotive audio applications such as head units and external amplifiers.

Specifically designed for the automotive market, the TAS5414 is a single-ended input amplifier, and the TAS5424 has differential input, enabling it to achieve higher dynamic range performance in a challenging board-signal-routing environment. The two amplifiers let designers select the optimum solution given their system performance and cost requirements.

Features:
TAS54x4 amplifiers deliver 90 percent power efficiency at normal radio listening levels for automotive audio systems.
Two TAS54x4 amplifiers provide eight channels of audio while generating less heat than a four-channel Class A/B-based system.
These devices eliminate the need for expensive shielding and other EMI countermeasures.
Both the TAS5414 and the TAS5424 are TS16949-certified.

TI Enables New Automotive Jukebox Market With High-Speed Ripping Capabilities

AV ReceiversAutomotive entertainment applications continue to incorporate features from the home. To meet this growing demand, TI announced high-speed encoding (HSE) application software and hardware based on its Aureus™ platform of high-performance audio digital signal processors (DSPs). This new functionality will enable advanced capabilities for applications such as automotive jukeboxes, automotive hard disk drive (HDD) navigation systems, home media servers and HDD-based stereo systems.

The HSE solution is ideal for applications such as a fast and inexpensive CD ripper to USB or NAND flash. Automotive jukeboxes are enhanced by supporting high-speed ripping from a CD loader to an HDD while simultaneously playing back content from USB, a DVD or HDD. In a car, the system could be simultaneously ripping and playing CDs for the driver while passengers in the back watch a DVD with multichannel or virtualized surround sound.

Features:
The DA710 offers outstanding HSE rates: 20X for ATRAC3 and 12X for MP3, Windows Media Audio (WMA), Advanced Audio Codec (AAC) and ATRAC3plus. (Rates listed are for stand-alone encode only.)
HSE functionality creates new product features, including automatic and transparent storage of content on a jukebox anytime a new CD is inserted.
System cost savings are enabled through software support of new interfaces to the DA7xx Aureus DSPs.
The high-speed encoding solution is built upon existing modular application software previously available for the Aureus digital audio processors for multichannel decoding applications.

New LVDS Serializer/Deserializer Less Than One-Third the Size of Competing Devices

TI has developed new low voltage differential signaling (LVDS) serializer and deserializer (SerDes) devices in a 5 mm x 5 mm QFN package. At less than one-third the size of competing devices, the SN65LV1023A serializer and SN65LV1224B deserializer save board space in a wide variety of applications, including wireless base stations, data communications backplanes, industrial systems, and video systems such as in-vehicle infotainment and video.



Features:
100-Mbps to 660-Mbps serial LVDS data payload bandwidth at 10-MHz to 66-MHz system clock.
No external components required for phase-locked loop.
Qualified for industrial temperature range from –40°C to 85°C.

OMAP™ Technology and TI Third Parties Drive Automotive Applications

Helping fuel the growth of the automotive infotainment market, TI announced key third-party relationships that will provide manufacturers with the tools to bring multimedia and communications applications to the center stack/head unit. TI partnerships will develop and integrate these technologies, providing a foundation for key applications such as hands-free connectivity, digital media middleware and global positioning system (GPS) technology. New applications leveraging technology from Gracenote, Stonestreet One, Trimble and Universal Electronics (UEI) represent the next evolutionary step for digital multimedia and communications in the car. These innovations are driven by TI's programmable OMAP™ technology for automotive applications, a dual-core digital signal processor (DSP) + RISC architecture designed to efficiently and cost-effectively implement automotive infotainment features.

Features:
UEI’s SimpleWare® Auto provides embedded software for the complete control and enjoyment of digital media in automotive products.
Gracenote offers an embedded music database facilitating the automatic recognition of CDs and digital music files, providing album and track titles and automatic playlists without requiring Internet access.
Stonestreet One provides Bluetopia®, a robust Bluetooth protocol stack with various user profiles for hands-free connectivity.
Trimble, a leading innovator in GPS technology, allows TI customers to minimize GPS integration cost, improve their development ROI and position themselves to take advantage of future positioning technologies such as Galileo.


Automotive Articles

Data and Audio Processing for HD Radio
John Gardner (Texas Instruments), Audio DesignLine
Feb. 6, 2006


The chicken-and-egg quandary "Will broadcasters make content before receivers are available or will receivers be made available before content is broadcast?" does not exist - at least as applied to terrestrial digital radio in the United States. Several ideas applied to HD radio broadcasts can speed mass adoption and time-to-revenue.

HD radio has distinct digital signal processing needs beyond the current analog radio of today. The added complexity in demodulating and decoding a base audio signal is coupled with the need to address data broadcasting and additional audio content. DAB and satellite provide an example to the HD radio market of how to effectively merge audio with data, as well as how broadcasters can effectively promote the technology. Beyond content and promotion, success in the HD radio market will come not only from choosing the correct platform that can handle HD radio signal processing but one that is flexible enough to take advantage of and exploit both audio and data features.


© 2006 Texas Instruments Incorporated, 12500 TI Blvd, Dallas, TX 75243

Technology for Innovators, the black/red banner, Aureus and OMAP are trademarks of Texas
Instruments. All other trademarks are property of their respective owners.