- What is the VSIP Development Platform?
- Who is Ateme and what is its role with the VSIP?
- What is the VSIP‘s official name and part
number?
- Who is TI targeting with the VSIP Development Platform?
- How will the VSIP benefit video surveillance system developers and video systems integrators? What capabilities will customers gain that they did not have with analog systems?
- Does this mean video surveillance system developers
and video systems integrators will have to completely overhaul
their systems?
- What features are included in the VSIP?
- How is the VSIP different from TI’s DMDK?
- What is the cost of the VSIP?
- Can I use my current emulator or do I need to
purchase a new emulator for use with the VSIP?
- When and where is the VSIP available?
- Who is the end user of the VSIP?
- What benefits can the end user look forward to
based on this technology?
- Where can I find more information on the VSIP?
1) What is the VSIP Development
Platform?
TI is introducing the new Video Security over Internet Protocol
(VSIP) Development Platform designed to address the growing demand
in the video security market for digital processing capability.
Built on the DM642-based board, the VSIP development platform is
a joint effort with solutions partner Ateme and targets security
camera OEMs, video system integrators and developers of new video
security technology. Developers will benefit from a programmable
digital video security solution that minimizes transmission bandwidth
and storage requirements, cuts costs by eliminating the expense
of bulky coaxial cables and, most importantly, incorporates intelligent
features such as the ability to capture relevant images and respond
only to significant events, among others.
Back to Top
2) Who is Ateme and what is its
role with the VSIP?
Ateme is headquartered in France and is one of the leading providers
of hardware and software solutions for video and signal processing
in the world. Ateme is a member of the MPEG-4 Industry Forum and
takes part in M4IF's interoperability tests.
Ateme and TI have a long-standing relationship and have been working
together since 1998. Ateme was instrumental in developing video
surveillance software incorporated in the development platform that
enables advanced features such as date and time reference, encryption,
noise filtering, alarm management and advanced motion detection.
Ateme also developed audio algorithms for the kit including MPEG-4
compression, ADPCM audio compression, RTP/RTSP video streaming and
more. Additionally, Ateme provides hardware customization services
for customer’s wishing to tailor their video surveillance
system.
Back to Top
3) What is the VSIP‘s official
name and part number?
Video Security over Internet Protocol (VSIP) Development Platform.
Part number - TMDSVSK6416
Back to Top
4) Who is TI targeting with the
VSIP Development Platform?
The development platform is targeted at security camera OEMs, video
system integrators and developers of digital video security technology.
It will enable them to quickly and easily migrate from analog to
intelligent digital video surveillance systems.
Back to Top
5) How will the VSIP benefit video surveillance system developers and video systems integrators? What capabilities will customers gain that they did not have with analog systems?
The rise of digital has uncovered many of analog’s shortcomings.
For instance, analog systems are maintenance intensive, offer no
remote accessibility and are notoriously difficult to integrate
with other systems.
Developers using the VSIP development platform will benefit from
a complete hardware and software platform, enabling them to build
intelligent security cameras that take advantage of a digital IP
network, while leveraging the real-time performance and flexibility
inherent in DSP technology.
Additionally, developers will benefit from the development platform’s
programmability allowing them to add highly differentiated features
never possible before with an analog solution. For instance, developers
can program cameras in such a way that when a condition sets off
an alarm, such as a car parked in a lot at a time not permitted,
the intelligent camera is able to zoom in, encode the images and
record specific images such as license plates and information of
interest. Other advanced features include camera control for pan,
tilt, encryption, alarm management and advanced motion detection.
Programming is further enhanced by the development platform’s
easy-to-use, open environment that speeds time to market.
Back to Top
6) Does this mean video surveillance
system developers and video systems integrators will have to completely
overhaul their systems?
No, implementing an IP-based video surveillance system does not
require throwing away trusted and already owned cameras. With IP-surveillance,
developers can still use existing equipment (cameras, lenses and
cables) in place through a network encoder. The network encoder
serves as an interface between several existing analog cameras and
an IP network. Developers also have the option to replace existing
equipment with a stand-alone IP camera that incorporates digital
functionality, allowing for reduced storage space and less operator
intervention. Either solution will benefit developers by providing
them remote accessibility, increased integration capabilities and
more intelligent capabilities.
Back to Top
7) What features are included in
the VSIP?
The platform includes board schematics, development hardware and
software and evaluation software.
Software includes:
- Code Composer Studio™ Development Tools v2.2
- Source code for multimedia framework
- Production algorithms:
- MPEG-4 video compression
- ADPCM audio compression
- RTP/RTSP video streaming
- PC supervision application
- TCP/IP stack
- Source code for device drivers:
- System software
- Noise filtering
- Audio/video compression
- Motion vector extraction
- Dating and referencing
Hardware includes:
- DM642 based board with CMOS sensor for IP camera
- One to four analog video inputs for the IP node version
- One on-board CCD sensor for the IP camera network
- One audio port
- Four I/O for different alarm sensors
Framework: source code for Multimedia Framework
Algorithms = evaluation-only libraries:
- MPEG4 simple profile encoder and decoder
- Audio decoder
- Networking stack
Back to Top
8) How is the VSIP different from
TI’s DMDK?
Unlike the DMDK, the VSIP development platform is specialized to
meet the specific needs of video surveillance OEMs. What differentiates
the VSIP from the DMDK is its MPEP evaluation code offering, networking
(client PC) demos and video surveillance-specific software.
Back to Top
9) What is the cost of the VSIP?
The complete VSIP Development Platform is available today and can
be ordered through TI distribution and Ateme for $14,995.
Back to Top
10) Can I use my current emulator
or do I need to purchase a new emulator for use with the VSIP?
Developers do not need to purchase a new emulator and can use their
current emulator with the development platform. However, if they
want to experience maximum performance and XDS560 class emulator
is recommended.
Back to Top
11) When and where is the VSIP
available?
The complete VSIP Development Platform is available today and can
be ordered through TI or Ateme distributors.
Back to Top
12) Who is the end user of the
VSIP?
End user consists of companies and organizations that utilize surveillance
systems such as large and small retail stores, jewelry stores, airports,
etc.
Back to Top
13) What benefits can the end
user look forward to based on this technology?
There are many end user advantages associated with migrating to
an IP-based video surveillance system including ease of use, remote
accessibility, advanced search capabilities, simultaneous record
and playback, minimal image degradation, improved compression and
storage, better integration potential and, most importantly, programmable
intelligence enabling advanced functionality.
Back to Top
14) Where can I find more information
on the VSIP?
You can find information at www.ti.com/vsipsp or at www.ateme.com.
Back to Top
|