Hardware & Software |
|
SimpleLink™ Wi-Fi® CC3000 |
SimpleLink Wi-Fi CC3000 is a wireless solution that simplifies the process of adding Internet connectivity to almost any MCU. The CC3000's low hardware requirements and unmatched integration enables Wi-Fi in many applications previously not possible. SimpleLink Wi-Fi CC3000 minimizes host microcontroller (MCU) software requirements which makes it the ideal solution for embedded applications using any low-cost/low-power MCU.
|
|
More |
|
|
Introducing TI's SimpleLink™ product family |
Building from more than a decade of proven leadership in the wireless connectivity space, TI recently unveiled the SimpleLink™ product family, the industry's widest portfolio of easy-to-use wireless connectivity technologies for low-power, low-cost embedded applications. The SimpleLink family includes self-contained wireless processors, aimed at enabling easy integration with any embedded system. |
|
Visit www.ti.com/simplelink for more |
|
|
TI introduces ZigBee® RF4CE advanced remote control solution |
TI's latest ZigBee® RF4CE remote control solution includes support for the upcoming ZigBee Input Device (ZID) profile, which enables mouse-like pointing functionality, keyboard and gesture- and touch-based input controls for consumer electronics such as TVs, set-top boxes and game consoles. TI's ZigBee RF4CE solution includes the royalty-free RemoTI™ 1.3 protocol stack with sample application software, an ETSI-compliant and FCC-certified nano USB module, and an associated Advanced Remote Control development kit.
|
|
For complete product details, visit:www.ti.com/rf4ce |
|
|
TI demos ZigBee Smart Energy 2.0 SoC with integrated ARM Cortex-M3 processor and memory |
TI recently announced the industry's first demonstration of a radio frequency (RF) system-on-chip (SoC) that integrates an IEEE 802.15.4 (2.4 GHz) radio, an ARM® Cortex™-M3 processor, dedicated Smart Energy (SE) 2.0 hardware security acceleration, and enough flash and RAM to run the ZigBee® IP stack and SE2.0 profile without requiring external memory. The CC2538 ZigBee SE2.0 SoC is aimed at products for the Smart Grid and remote sensor connectivity to the Internet, and will enable simplified, cost-effective development of SE2.0 compliant applications such as electricity, gas or water smart meters and in-home displays. |
|
More |
|
|
New FW1.3.0 released for PurePath Wireless Audio |
New features include, but are not limited to, support for microphone(s), standby mode, antenna diversity and single button / proximity pairing.
|
|
More |
|
|
Technical Documents |
|
TI NFC Technology Simplifies Bluetooth Pairing |
Bluetooth® pairing usually involves some level of user interaction to confirm the identity of the user and/or the devices themselves. There are many pairing mechanisms available across the versions of Bluetooth. This process is typically lengthy and sometimes confusing to the user. This application report is aimed at showing TI technology developers details on implementing a simplified pairing scheme method outlined by the NFC Forum using an MSP430F5529 (a TI ultra-low power MCU), a TRF7970A (a TI NFC transceiver IC), and an CC2560 (a TI Bluetooth radio IC). |
|
More |
|
|
|
RF6505-CC2530 range extender reference design |
The RF6505-CC2530 reference design is a range extender design for the 2.4GHz ISM bands and contains schematics and layout files for the RF6505-CC2530 evaluation module. The reference design demonstrates how to integrate TI's CC2530/CC2531 and the RF6505 RF Front End from RF Micro Devices, and includes techniques for decoupling and RF layout. |
|
More |
|
|
|
CC1120+CC1190 868 MHz Reference Design |
The CC1120-CC1190EM 868MHz reference design contains schematics and layout files for the CC1120-CC1190EM 868MHz evaluation module. The RF section has been designed and characterized for operation in the 869.4 - 869.65 MHz sub-band (g3). The maximum output power is +27 dBm @3.0V and the sensitivity is improved 3 dB compared to a CC1120 stand-alone solution. |
|
More |
|
|
AN112 Using CC1190 Front End with CC112x Under EN300220 |
This application note outlines the expected performance when using a CC1101-CC1190 design under EN 300 220-1 V2.3.1 in the 869.4-869.65 MHz sub-band (g3). The maximum output power is +27 dBm @3.0V and the sensitivity is improved 3 dB compared to a CC1120 stand-alone solution. |
|
More |
|
|
Developer’s News |
|
9Solutions Bluetooth Low Energy Indoor Navigation and Real Time Locating System |
At CES 2012 9Solutions and TI demonstrated the first real time Bluetooth low energy-based indoor navigation and tracking system using Apple iPhone 4S and 9Solutions' Lone Worker Protection ID-Badge Tag and uTag product line. The 9Solutions IPCS Bluetooth low energy product line utilizes TI's CC2540 Bluetooth low energy system-on-chip.
Watch a demo video of 9Solutions IPCS here |
|
More |
|
|
|
Other News |
|
|
|
Events |
|
Enabling M2M with Wi-Fi - join TI and LSR at Arrow M2M Seminars |
A common issue faced today is easily accessing information, diagnostics, or controlling machines remotely. To expand the capability of products traditionally connected via a wired interface, engineers are looking for ways to wirelessly monitor and control systems from any location. Furthermore, users are looking for this accessibility without the need for new hardware or controllers, or years of expertise. TI and LS Research have partnered to create an innovative Wi-Fi® solution to address these design challenges. Discover how this solution expands machine functionality while simplifying your design process. |
|
Visit the M2M Seminar Series website for more information and to register for the seminar nearest you. |
|
|
Join TI at Mobile World Congress 2012, Barcelona, Feb 27th - March 1st |
Experience the art and science of mobility! Meet TI experts at Stand 8A84, Hall 8 -and experience how our technology is empowering the mobile landscape. See products and demonstrations featuring wireless connectivity solutions, OMAP™ mobile processors, power management, communications infrastructure, high-speed products and DLP® projection technology.
Learn more about TI's Mobile World Congress plans online on www.ti.com/mwc2012 (please bookmark and stay tuned for more), and plan to stop by our booth in Barcelona. See you there! |
|
|
|
|
Visit TI’s E2E™ Community and interact with your peer engineers, TI engineers, and other experts in order to ask questions, share knowledge, explore ideas, and help solve problems.
Product Information Centers
|
|
|
|