Low-Power RF eNewsletter December 2008
Texas Instruments

Dear %%FIRST_NAME%% %%LAST_NAME%%

Below are the latest updates from Low-Power RF:

Software and hardware:
•  New CC2520EMK Evaluation Module Kit
 
•  New Design Note: DN114 Test Signals for debug purpose in CC111xFx CC251xFx and CC243x
 
•  Updated: CC1101 Data Sheet
 
•  CC1101EM announcement
 
E2E online community – what are engineers discussing right now?
•  Compiler Support
 
•  ESD protection scheme
 
•  Role of ZigBee coordinator
 
•  CC430 Blog – Join the journey towards the new CC430 technology platform
 
Developer news:
•  Radiocrafts provides a wireless M-Bus gateway with partner Sensinode
 
•  Amber Wireless' AMB8425-M Wireless M-Bus Radio Module 868 MHz
 
•  Sensinode launches Metering Bus technology with TI Low Power RF radios



NEW – CC2520EMK Evaluation Module Kit
The CC2520EMK, which is an add-on kit to the CC2520DK, is now available. The CC2520EMK contains 2 CC2520EM plug in modules and 2 antennas. The modules can be plugged into the SmartRF05EB or the CCMSP-EM430F2618 board that is included in the CC2520DK. The board can also easily be connected to other microcontrollers, allowing fast prototyping with the CC2520 transceiver.
More



NEW – DN114 Test Signals for debug purpose in CC111xFx CC251xFx and CC243x
More
 


UPDATED CC1101 Datasheet
The datasheet has been formatted and edited, and important information like wireless MBUS compliance, application circuit updates, antenna solutions that was only available in application and design notes, have been added with links to the respective documents. Further, information regarding variation in output power, sensitivity and current consumptions over conditions has been added.
More


CC1101EM announcement
The current revision of the CC1101EM reference design uses Murata LQG15 series multilayer inductors and the maximum output power is +10 dBm. Using Murata LQW15 series wire-wound inductors the CC1101 output power is +12 dBm @868 MHz (33.3 mA) and +11 dBm @ 915 MHz (32.6 mA). For the same output power, the current consumption in transmit mode is lower with the wire-wound inductors compared to using the multilayer inductors (30.0 mA vs 32.3 mA @+10 dBm, 868 MHz). Furthermore, the harmonics emission is significantly reduced when using wire-wound inductors. The sensitivity is improved by 1 dB when using wire-wound inductors. The CC1101EM-868/915 MHz reference design and the CC1101 datasheet will be updated using wire-wound inductors.


CC430 Blog – Join the journey towards the new CC430 technology platform
The CC430 Blog keeps you updated on the new Low-power RF and MSP technology. The Blog is updated on a monthly basis with information on relevant application areas, energy harvesting, technical information and more.
More


Radiocrafts provides a wireless M-Bus gateway with partner Sensinode
Radiocrafts and Sensinode have launched a Wireless M-Bus gateway targeted for the AMI ( Automatic Metering Infrastructure) and WSn (Wireless Sensor Network). This solution provides wireless acces for many IP (Internet protocol) based sensors eliminating the huge cost of wired installations in the emerging process monitoring vertical market.
More


Amber Wireless Germany launches Wireless M-Bus AMB8425 module
The Metering event in Amsterdam this fall has shown that there is increasing demand for AMI standards in Europe. Wireless Mbus modules are now available for sale through TI Low Power RF developer Amber Wireless. MSP430 developers in Europe who are working with MSP, will like the fact that they can share the processor on the AMB8425 or can use the transceiver AMB8400 in combination with Amber Wireless M-Bus stack.

Advantages of Amber's solution:
  • Software is written for MSP.
  • Two board solution, digital part with software and transceiver module AMB8400
  • Customer can use Amber software and hardware. One stop solution
  • Amber is member of the Open Metering Group and member of the AG1. This group is responsible for the wireless protocol
Selling price of the AMB8420-1 at 100k is 2,90 Euros

More


Sensinode launches Metering Bus technology with TI Low Power RF radios
Wireless MBUS is a growing standard for the meter industry in Europe. Sensinode software and wireless "nanorouter" technology provide a compelling solution for European AMI developers interested in enhanced capability of linking IP (internet protocol) wireless sensors using Sensinode nanorouter technology.
More


Low-Power RF Developer Network
TI's extensive network of low-power RF development partners can help you speed up your application development. The network comprises recommended companies, RF consultants and independent design houses that provide a variety of hardware module products and design services, including:
  • RF circuit, low-power RF and ZigBee design services.
  • Low-power RF and ZigBee module solutions and development tools.
  • RF certification services and RF circuit manufacturing.
  • Online search tool to determine suitable RF development partners.
More


Customer Support Contact Information
Product Information Center - Americas
Product Information Center - Europe, Africa, Middle East
Product Information Center - Asia/Pacific
Product Information Center - Japan


To ensure delivery to your inbox, please add tiprime@dlep14.itg.ti.com to your address book or safe sender list. 

The platform bar is a trademark of Texas Instruments. All other trademarks are the property of their respective owners.

%%DYN_FOOTER%%