Dear %%FIRST_NAME%% %%LAST_NAME%%
Below are the latest updates from Low–Power RF |
|
| CC2530 Second generation system–on–chip for ZigBee®, RF4CE, Smart Energy, and IP applications |
| The new CC2530 is a true system-on-chip solution tailored for IEEE 802.15.4, ZigBee, ZigBee RF4CE and Smart Energy applications. With its large flash memory of up to 256 KB, the CC2530 is ideal for ZigBee PRO applications. The 64 K and up versions will support the new RemoTI™ stack for ZigBee RF4CE, which is the industry's first ZigBee RF4CE-compliant protocol stack, and larger memory sizes will allow for on-chip over-the-air-download to support in-system reprogramming. |
| More |
|
| CC1100E low–power Sub–1 GHz RF Transceiver for China and Japan frequency bands |
| TI has just launched the CC1100E which is a dedicated RF transceiver for metering applications in China using the 470-510 MHz band and RFID applications in Japan using the 950-960 MHz band.
The CC1100E has the following characteristics:
| • |
Covers 470-510 MHz and 950-960 MHz frequency bands |
| • |
2kV ESD protection on all pins |
| • |
Code, pin and register compatibility with CC1100 and CC1101 |
|
| More |
|
| TI introduces RemoTI™ network protocol for ZigBee® RF4CE consumer electronics applications |
| RemoTI network protocol is a low-cost, feature-enriched solution including TI's best-in-class CC2530 IEEE/802.15.4 system-on-chip and software stack. A comprehensive development kit from TI provides all hardware, software and tools necessary to evaluate, develop, test and debug an RF4CE-compliant product, enabling designers to quickly bring RF remote controls to market. |
| More |
|
| New USB libraries for CC1111Fx, CC2511Fx and CC2531Fx |
| Our USB Firmware Library with software examples has been updated to Revision B. The new release features: Added support for CC2531, HID example emulates simple mouse and keyboard operations using a SmartRF04EB or SmartRF05EB, CDC example with RF Modem/Virtual UART, MRFI radio link layer, SW tested against USB Command Verifier, passing Chapter 9 and HID tests, HID and RF Modem SW examples rewritten from scratch, Documentation split in software and hardware manuals, Tested on Windows XP SP2/SP3, Windows Vista SP1 and GNU/Linux (Ubuntu 9.04), Bug fixes to the USB Firmware Library, CDC class and HID class.
The software and the documentation can be downloaded from the following web pages:
http://focus.ti.com/docs/toolsw/folders/print/cc2530dk.html#Support%20Software
http://focus.ti.com/docs/toolsw/folders/print/cc2511emk.html#Support%20Software
http://focus.ti.com/docs/toolsw/folders/print/cc1111emk868-915.html#Support%20Software |
|
| New revision of CC1101 data sheet |
| Using wire wound inductors improves maximum output power to +12/+11 dBm at 868/915 MHz, reduces the current consumption for a given output power, reduces the harmonics emission, and improves the sensitivity by 1-2 dB compared to using multi–layer inductors. The new revision of the data sheet includes electrical parameters for operation at 868/915 MHz when using wire wound inductors. |
| More |
|
| Updated CC1110EM 868 and 915 MHz reference design |
| The CC111x RESET_N pin is sensitive to noise and can cause unintended reset of the chip. The CC1110EM-868 MHz reference design has been updated with an external RC filter with values 1 nF and 2.7 kohm close to the RESET_N pin. |
| More |
|
| Updated CC1110EM 433 MHz reference design |
| The CC111x RESET_N pin is sensitive to noise and can cause unintended reset of the chip. The CC1110EM-433MHz reference design hasl been updated with an external RC filter with values 1 nF and 2.7 kohm close to the RESET_N pin. |
| More |
|
| Updated CC1110EM 315 MHz reference design |
| The CC111x RESET_N pin is sensitive to noise and can cause unintended reset of the chip. The CC1110EM-315MHz reference design hasl been updated with an external RC filter with values 1 nF and 2.7 kohm close to the RESET_N pin. |
| More |
|
| New CC2511 USB nano dongle reference design enables ultra compact USB designs |
The CC2511 USB nano dongle reference design shows how to make an ultra compact USB dongle with the CC2511 system-on-chip, using a PCB antenna and single sided components mounting.
The reference design contains schematics and layout files for the CC2511 USB nano dongle. The reference design demonstrates good techniques for decoupling and RF layout in miniaturized PCB designs with the CC2511.
This is a 4-layer reference design with a compact balun and antenna integrated in the PCB. |
| More |
|
| Third European ZigBee Developers' conference |
| After the great success of the first two European ZigBee Developers' Conferences in 2007 and 2008, the ZigBee Alliance will hold their 3rd European ZigBee Developers' Conference (EuZDC) from June 30 to July 1, 2009 at the NH Hotel Munich–Dornach (Germany). Texas Instruments will participate again this year so don't miss this opportunity to learn about the actual and future status of the ZigBee development, to get to know hardware and software products, and to get acquainted with the development process. |
| More |
|
| MSP430 868⁄915 MHZ Wireless Target Board available from Amber Wireless |
| The AMB8423 is the 868⁄915 MHz-version of the 2.4 GHz radio module of the TI eZ430-RF2500. The AMB8423 uses an 868⁄915 MHz CC1101 wireless transceiver instead of the 2.4 GHz CC2500 found on the eZ430-RF2500T. The board also features a modified antenna design to support the new frequency band. |
| More |
|