Design Support

TVP5146 FAQ

The following frequently asked questions (FAQ) on the TVP5146 are from a variety of sources covering many aspects of the device itself, its features, application, and EVM. This document is organized into sections related to different areas of the TVP5146. Questions related to multiple areas are shown in each area along with the corresponding answer. The size of this document and the number of questions covered may make it difficult to locate an FAQ. If this is the case, try using the Search tool to locate specific words associated with the FAQ. Questions not covered in this document may be available by referring to the TVP5146 Data Manual, SLES084, as well as the various application notes and user's guides available at http://www.ti.com.



Bookmark and Share