TMS320C30 Addressing up to 68 Gigawords
The primary bus of the TMS320C30 has 24 address lines, which allows addressing of up to 16 megawords of memory. The expansion bus has 13 address lines, which allows addressing 8 Kwords. Using the techniques shown in this document, they can be used together to address a larger memory space of up to 68 gigawords.
|