TMS320C6000 HPI to PCI Interfacing Using the PLX PCI9050 (Rev. C)
This application report describes an interface between the Texas Instruments TMS320C6000™ DSP host port and the PLX Technology PCI9050 (PCI9052), the PCI interface chip. The PCI9052 is functionally the same as the PCI9050. The only difference between these two devices is that the PCI9052 is somewhat faster than the PCI9050.
This application report includes a diagram showing connections between the two devices, PAL equations, and verification that timing requirements are met for each device (using tables and timing diagrams).
|