TMS320F240 DSP Solution for Obtaining Resolver Angular Position and Speed
This application report presents a TMS320F240 DSP solution for obtaining the angular position and speed of a resolver.
A resolver is an absolute mechanical position sensor used, for example, in servo applications. It is basically a rotating transformer. The sinusoidal input reference is amplitude modulated with the sine and cosine of the mechanical angle, respectively. These two output signals have to be decoded to obtain the angular position.
For decoding the resolver output signals, a basic method is introduced. It utilizes undersampling and an inverse tangent function. To achieve a higher angular resolution an improved method, which adds oversampling techniques is used. Due to an integral invariant filter, which is a combination of an IIR and FIR filter, the digitized angular position does not suffer any velocity lag.
Thanks to its peripherals, the TMS320F240 DSP can be ideally used for decoding the two resolver output signals as well as for generating the input reference frequency. The hardware interfacing of the resolver to the TMS320F240 is shown and the software realization of the improved method on the TMS320F240 is documented. All software routines are C-compatible. The angular resolution achievable with the TMS320F240 is up to 14 bits, at a CPU loading of 13%.
Thus, the TMS320F240 will eliminate the cost for the external resolver-to-digital conversion IC, since the algorithm runs in addition to the motor control task.
|