Migrating from TMS320C6211B/C6711/C6711B and C6713 to TMS320C6713B (Rev. H)
This document describes issues of interest related to migration from the Texas Instruments TMS320C6211B/C6711/C6711B GFN package and TMS320C6713 GDP package to the TMS320C6713B digital signal processor (DSP) GDP package. The objective of this document is to indicate differences between these devices. Functions that are identical between these devices are not included. For detailed information on the specific functions of any of these devices, refer to the device data sheets. Migration issues from C6211B/C6711/C6711B and C6713 to C6713B are indicated with the following symbols, which are included at the beginning of each section:
[H] Means hardware modification is required. [S] Means system/software modification is required. [D] Means the C6211B/C6711/C6711B, C6713 and C6713B are different (usually due to added features on the C6713B), but no modification is necessary for migration (that is, the devices are different but compatible). With detailed description in this document, migration and development of C6713B systems can be accomplished with ease. For information about migrating from C6211B/C6711/C6711B to C6713B see section 1 for details. A summary of differences between C6713 and C6713B is also presented for C6713 and C6713B system migration; see section 2 for details.
|