Design Support

Migrating from TMS320VC5510 to TMS320VC5502

This document describes issues of interest related to migration from the TMS320VC5510 to the TMS320VC5502. The objective of this document is to indicate differences between the two devices. Functions that are identical between the two devices are not included. For detailed information on the specific functions of either device, refer to the following data manuals and reference guides: the TMS320VC5510 Fixed-Point Digital Signal Processor Data Manual (SPRS076), the TMS320VC5502 Fixed-Point Digital Signal Processor Data Manual (SPRS166), the TMS320C55x DSP CPU Reference Guide (SPRU371) and the TMS320C55x DSP Peripherals Reference Guide (SPRU317).



Bookmark and Share