TMS320C6747/45/43 Complementary Products
This article has been contributed to the TI DaVinci™ and OMAP™ Developer Wiki. To see the most recently updated version or to contribute, visit this topic at:
http://wiki.davincidsp.com/index.php/C6747/45/43_Complementary_Products .
This Wiki article serves as a repository of complimentary devices that can be paired with the C6747/45/43 floating-point digital signal processors (DSPs) when integrating the device into a system. The complementary products listed here serve a wide range of functions such as:
- Providing basic support functions for the DSP (power, clocking, etc.)
- Expanding the interface options beyond the on-chip peripherals
- Creating the link between the digital domains on the DSP to the system's analog/physical domains
The complementary products are organized into functional categories, with the goal of showing several options and their respective benefits.
Applicable Devices:
|