September 2, 2009
New Eclipse-based Code Composer Studio™ IDE enables customers to develop embedded applications for less than $100
New Code Composer Studio v4 combines the advantages of the Eclipse software framework with advanced embedded debug capabilities resulting in a compelling feature rich development environment for embedded developers.
CCStudio v4 is compatible across multiple processors in TI’s broad embedded portfolio, including microcontrollers, digital signal processors and ARM-based OMAP™ application processors. This supplies a common environment that simplifies development across a host of processor types. The IDE offers a number of low cost JTAG options including an XDS100 class emulator and corresponding CCStudio license for less than $100, which provides a low-cost entry point for development and allows users to later upgrade to higher performance debug solutions if necessary. Learn more.
July 21, 2009
Connectivity made smarter via new MSP430 MCUs with embedded full-speed USB and the world’s leading ultra-low power consumption
The new F55xx family offers the world’s leading ultra-low power consumption combined with high-performance analog and other smart integrated peripherals. Helping cut the power cord, the F55xx MCUs are well-suited for cost-sensitive applications including portable measurement for medical, industrial, and health and fitness, as well as consumer electronics and a broad range of other applications.
F55xx MCUs are priced from sub-$1 in large volumes. All are instruction set compatible with the entire MSP430 platform. Learn more.
April 20, 2009
MSP430FG47x MCUs provide ultra-low power, high performance and analog peripherals for efficient development of low-cost medical products
The FG47x MCUs offer on-chip integration of the complete signal chain, reducing design complexity and resulting in significant space and cost savings. These devices will help developers improve the quality and accessibility of healthcare through products such as blood glucose meters, digital thermometers, pulse oximeters, blood pressure/heart rate monitors.
FG47x MCUs are available and fully compatible with the MSP-FET430U100 and the MSP-FET430UIF flash emulation tool kits, speeding development and time to market.
Learn more:
March 19, 2009
MSP430 Teaching ROM
MSP430 Teaching Material Texas Instruments is proud to be a leader in helping those who are interested in learning microcontrollers and those who want to learn how to make stuff with electronics. To further this goal, we are now releasing a free teaching CD for those who are interested.
This CD was specifically designed to help professors create and adapt courses for the MSP430 architecture, but it can be used any way that the user would like as it provides modular, open source content on topics ranging from general information about microcontrollers to advanced robotics labs. It is useful for anyone looking to learn the MSP430 architecture and it discusses all the MSP430 peripherals with over a dozen labs and 15 chapters.
You can request
a CD by mail or download today
(400 MB file).
February 9, 2009
MSP430F5438 Experimenter's Board Makes Designing Easier Than Ever
The EXP430F5438 features a socket to drop in the latest F5438 devices, as well a dot-matrix LCD display, 3-axis accelerometer, microphone, audio out, USB connectivity, support for all TI-LPRF EM boards, and out of the box support for the ZigBee Pro stack. Learn More
January 19, 2009
MSP430 Solar Energy Harvesting Development Tool Enables Perpetually Power, Battery-less Applications
The eZ430-RF2500-SEH is a complete Solar Energy Harvesting development kit to help create a perpetually powered wireless sensor network based on the ultra-low-power MSP430 microcontroller. It features a custom solar panel, energy conversion circuitry and tiny thin-film rechargeable batteries capable of 400-1000 wireless transmissions with no light source to harvest energy from. Learn
more.
November 11, 2008
The all new CC430 combines leading MCU and RF technology Bringing personal and industrial wireless networking to the mass market
Announcing the NEW CC430 technology platform offering the industry’s lowest power, single-chip radio-frequency (RF) solution for microcontroller- (MCU) based applications. By making RF design easy, small, performance-rich and power-efficient, the CC430 platform helps advance applications including RF networking, energy harvesting, industrial monitoring and tamper detection, personal wireless networks, automatic metering infrastructure (AMI) and heat cost allocators. Learn
more.
August 19, 2008
Energy harvesting becomes reality with AdaptivEnergy's wireless, remote sensing solution based on TI ultra-low power technology
AdaptivEnergy has developed a demonstration kit using Joule-ThiefTM
technology to harvest energy and power the MSP430 microcontroller and
RF technology to collect data, control the operation of a system or send
sensed data to central collection sites. The Joule-Thief energy harvesting
device is based on AdaptivEnergy's Ruggedized Laminated Piezo (RLP®)
technology, which enables compact energy harvesting modules to power
applications such as wireless sensors. These wireless sensors could be
used to gather ambient intelligence to detect and report critical conditions
in factories, automobiles, office buildings, homes and other environments
- all without wiring or batteries. Learn more. |