|
MINNEAPOLIS, MN (June 2, 2008) - As the desire to offer consumers smaller, easier-to-use medical products grows, Logic and Texas Instruments Incorporated (TI) (NYSE: TXN) today released a new development kit specifically designed to quickly bring new medical products to market. The new ZoomTM Medical OMAP35x Development Kit and companion System on Modules (SOMs) use TI's OMAP35x processor to provide developers with a cost-effective, compact way to design and produce medical, industrial and other embedded applications. For more information, see www.ti.com/medicalevmpr.
The development kit allows medical product companies to easily develop sophisticated integrated medical devices with advanced graphical user interface, smart and real-time physiological processing, and wired and wireless connectivity options for patient monitoring and data logging applications. All of this is accomplished with a low cost, highly flexible software development environment, and the SOM design of the medical development kit provides rapid manufacturing to help avoid additional trials or product releases.
"TI's integrated circuit innovations empower customers to make advanced medical devices that are more flexible, affordable and accessible," said Srik Gurrapu, marketing and business development manager, Low-Power Medical Processors, TI. "The SOM module based on the OMAP35x platform will help medical customers quickly begin development and take advantage of a unique combination of high performance and very low power consumption. Having the same SOM module in the development kit greatly reduces development time investment and risk for medical customers."
OMAPTM processors drive innovative and easy-to-use medical products
TI's OMAP35x processors that drive these modules provide laptop-like performance at handheld power levels, with an integrated ARM® CortexTM-A8 core, TMS320C64x+TMdigital signal processor (DSP), 2D/3D graphics engine and video accelerators. By combining this high-performance processor with the memory and connectivity (wired and wireless) subsystems and a full operating system into an off-the-shelf OMAP35x SOM, developers can take a superior end-product to market quickly and easily. For more information on OMAP, see www.ti.com/omap35xpr.
"The OMAP35x SOM will highly benefit the medical and other embedded markets," stated Kurt Larson, Product Marketing Manager for Logic. "Since the OMAP35x processors are based on high-performance, low-power ARM processors, customers can realize significant gains in horsepower and peripheral functionality, even within the tightest power constraints."
The OMAP35x processors in the 0.4mm pitch BGA package enables Package-On-Package capability to mount the memory on top of the OMAP35x processor. This means equipment manufacturers can deliver the smallest form factor and lowest power for medical and other embedded applications. These packages often require complex design and manufacturing, but the SOM module minimizes these challenges.
System on Modules (SOM) accelerate time to production
Logic has placed the OMAP35x processor onto a SOM-LV Type III form factor module. The OMAP35x SOM, measuring 31 x 76.2 x 7.4 mm (1.22 x 3 x 0.29 inches), is small enough to fit into almost any application, yet includes all necessary development interfaces for today's embedded products, including Bluetooth® 2.0 + EDR, 802.11b/g wireless Ethernet, USB 2.0 OTG, 24bpp TFT LCD controller, and four-wire touch screen.
In addition to providing the latest technologies, a variety of different operating systems can be used with the Zoom Medical OMAP35x Development Kit, including Linux, Windows® CE and Green Hills operating systems. The multiple BSPs allow developers to select an OS that best supports their needs and costs.
Price and availability
The Zoom Medical OMAP35x Development Kit (TMDXMEVM3503-L) is available in limited quantities now and will be broadly available in 3Q08 for $995.
The OMAP35x SOMs will be available for use in production quantities through Logic's distribution network. Standard SOM configurations are listed below:
- SOMOMAP3530-10-1672IFCR
- OMAP35x processor, 128 MB DDR SDRAM, 256 MB NAND flash, 8 MB NOR flash, 802.11b/g, Bluetooth 2.0 + EDR, wired Ethernet, audio, touch
- 5K unit suggested resale $229
- SOMOMAP3530-10-1670EFCR
- OMAP35x processor, 128 MB DDR SDRAM, 256 MB NAND flash, audio, touch
- 5K unit suggested resale $175
Both modules are in the SOM-LV Type III form factor (31 x 76.2 x 7.4 mm). For more information on Logic's standard SOMs visit www.logicpd.com/products/som/. For information about custom SOM configurations, please contact Logic sales: product.sales@logicpd.com.
About medical products from Texas Instruments
TI is helping shape technology to improve the quality and accessibility of medical equipment to revolutionize healthcare in the 21st century and beyond. With its full range of analog and DSP products, from building blocks to complete solutions, plus systems insight, global support infrastructure, advanced process technology and medical industry involvement, TI is helping make innovative medical electronics more flexible, affordable and accessible. TI's experience in diverse markets, such as wireless communications, consumer electronics, automotive and aerospace, enables engineers to meet increasing needs for higher speeds, higher precision, lower power and smaller equipment, while maintaining the high standards for quality and reliability that the medical market demands. For more information, please visit www.ti.com/medical.
Back to Top |