Press Center

News Releases

Image Library

Press Contacts

New Eclipse-based Code Composer Studio™ IDE from Texas Instruments enables customers to develop embedded applications for less than $100

HOUSTON (Sept. 2, 2009) - As software design and debugging represents the majority of development cost and time for many applications, efficient design tools play a critical role in managing project cost and deadlines. To simplify development while accelerating identification, analysis and resolution, Texas Instruments Incorporated (TI) (NYSE: TXN) today announced the availability of Code Composer Studio v4, a major upgrade to its industry-leading integrated development environment (IDE) based on the Eclipse open source software framework (www.ti.com/ccs4-prprod).

CCStudio v4 is compatible across multiple processors in TI's broad embedded portfolio, including microcontrollers, digital signal processors and ARM-based OMAPTM application processors. This supplies a common environment that simplifies development across a host of processor types. The IDE offers a number of low cost JTAG options including an XDS100 class emulator and corresponding CCStudio license for less than $100, which provides a low-cost entry point for development and allows users to later upgrade to higher performance debug solutions if necessary.

The open source Eclipse framework is quickly becoming the industry standard for IDEs, providing an excellent software architecture where developers can leverage the existing Eclipse community and the integration of a wide selection of third party plug-ins to speed troubleshooting, analysis and profiling of embedded designs. CCStudio v4 combines the advantages of the Eclipse framework with advanced embedded debugging capabilities developed by TI, along with multi-processor debugging and a comprehensive windowing solution.

Code Composer Studio v4 key features and benefits:

  • Superior code development environment speeds design and troubleshooting with an advanced editor and features such as code completion, code folding, local history of source changes, markers and the ability to associate tasks with source lines. Developers can also directly view images and video in their native formats.
  • Advanced GUI framework simplifies data and project management through the creation of perspectives with full customization of menus, toolbars and 'fast views' that enable developers to define the functionality and views appropriate to specific tasks, such as editing or debugging a program across multiple processors.
  • Multi-processor debugging intelligently manages status and information from multiple cores without the confusion that arises when each core requires its own separate debugger. More than 1200 third-party plug-ins support product development including static code analysis, source code control, modeling and scripting development.
  • Flexible project environment gives developers control over the compiler and DSP/BIOSTM version used with each individual project allowing projects in maintenance mode to continue to use the tools they were deployed with while enabling new projects to take full advantage of the latest improvements in technology.
  • Debug server scripting interface enables the automation of common tasks such as code validation and profiling.
  • Update manager tool automatically manages tool updates.

Pricing and availability

There are a variety of pricing options depending on the type of license needed. Developers can download a free 30-day trial to quickly evaluate different processors and begin development.

Find out more about TI's extensive Code Composer Studio portfolio by visiting the links below:


Back to Top